Other Parts Discussed in Thread: TPS92691, TPS92692
Hi All,
I have designed an application using the TPS9262-Q1. The application drives two high power LEDs. There are two drivers on the PCB , one for each LED. The LEDs work at 32V and 0.6A each.
The design seems to work fine ,it drives the right current. The problem is that it is making a noise. When we power up just one driver it doesn't make any noise, but when both are driving current at the same time it makes a noise.
I understand that if both drivers individually don't make any noise the circuit should be working fine. I don't know why when both are switching it is making a noise. Could it be because both are switching at the same time but asynchronized and then it is making the PCB vibrate?. Could it be any other reason other like coupling, resonance of inductors ( but individually don't make noise) or any other thing?
Any help would be very appreciated.