This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616EVM: Test issue

Part Number: BQ24616EVM


Hi Team,

I encountered some problems while testing the 24610EVM board,

Cannot use electronic load and power supply to simulate battery

My input is a 24V power supply, and the BAT is connected to the electronic load CV mode (18V) and power supply (17V). I want to simulate the battery charging process, but I found that STAT1 and STAT2 on the EVM are not bright(CE is bright), and the current read by the electronic load is also very small. I did not enter the charging state when I judged, so I want to know whether my setting like this can simulate the process of battery charging? In addition, I did not provide 1.8v for TS, will it not work?

Thanks

Z