Can the output pin (Q) tolerate an externally-applied voltage? In this case Vin would be 9V, the TL4242 would be disabled (PWM = 0V), but 6V would be applied to Q. Is this ok?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the output pin (Q) tolerate an externally-applied voltage? In this case Vin would be 9V, the TL4242 would be disabled (PWM = 0V), but 6V would be applied to Q. Is this ok?
Hi david,
What do you mean the "when I=0V" it is floating or connetc to the ground?
BR
Sean
It would be when one of the input power supplies is not present. In my case that rail is quickly discharged down to about 2V when the input is removed and then slowly down to 0V. So I think the answer to your question is that the input is connected to ground. It certainly is not floating.
Hi David,
I'm sorry that I don't think it can be power from the "Q" pin when "I" pin is connected to ground since there is a biode diode for the internal FET.
BR
Sean
Hi Dave,
That is the simplifiere block diagram and it needs to test to confirm. Let me check with the internal team and reply to you later.
BR
Sean