Other Parts Discussed in Thread: TPS61094
Dear Team,
Do we have any low iq solution can meet spec in one chip as below?
case 1 : input voltage 1.8V,output : 4V , output current 300mA
case 2 : input voltage 1.8V,output : 3.3V , output current 600mA
If not, could you help to suggest 2 solutions (low iq) can meet each 2 spec.
Thanks a lot.
Jimmy