Other Parts Discussed in Thread: UCD9248,
Dear TI team
Our customers are using UCD9248 and PTD08D210W as a set.
I have a question about the input pin of the PWM signal of PTD08D210W (the module on which UCD7240 is installed).
1. When the PWM signal input to the PWM-A (PWM-B) pin of PTD08D210W (UCD7240) becomes 0V, it is good to recognize that the output A (output B) becomes 0V even when the input voltage is 0V or more. Is it?
2. If the PWM-A and PWM-B pins are floating, or if there is a momentary noise from the PWM-A and PWM-B low states, will the PWM-A and PWM-B pins be low? ..
(I thought that there was an internal pull-down on the input pins of PWM_A and PWM_B, so I asked.)
Best Regards,
Y.Ottey