Hi
I have connected two LM66100 in parallel for
The Vin1 is 3.4 - 4.8V.
Vin 2 is 5.5V.
The voltage source is slected by CE from a microcontroller with Logics : High (2.6V) and Low(0V). Datasheet seems to say that to TURN OFF, CE should be higher than Vin. Please clarify.
Thanks.
Siva