This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548B22: Ramp Setting

Part Number: TPS548B22


Hi Expert,

Customer used TPS538B22 with condition 12Vin to 0.8Vout/20A, Fsw=650Khz.

From DS table 7 recommendation, Ramp = R/2 for Vo=0.8V but in real testing, they could pass bode plot PM>45deg criteria by increasing Rx2 or Rx3. Do you have any concerns to do that? 

Thanks,

Allan

  • Hi ,

    The table is just giving a guideline or starting point. If the customer is satisfied with the phase margin at the higher ramp settings, then there is no issue going to the higher settings. You can see from Section 8.2.3.3.1 in the datasheet that there is a relationship between minimum output capacitance for stability, ramp time constant and other design variables, so you may be stable with higher ramp time constant for a given condition so long as the stability criteria is satisfied.

    Regards,
    Kris