Other Parts Discussed in Thread: GPCCEDV, EV2400
I have a Battery Pack with BQ3060 Fuel Gauge. I am having a problem where the following registers do not seems to be updating:
Remaining Capacity 0x0F
Absolute State of Charge 0x0E
RSOC
This is even after multiple cycle where battery has drained. The battery pack is designed to power a motherboard after main power source looses the AC power. Motherboard circuitry includes CPU, DRAM DIMMs,PCI-e devices which can consume about 250W of power. When battery is supplying power, I would expect that battery capacity will go down significantly. The pack capacity is 1000mAh.
For instance RM register always shows 91%. and even FCC does not seems to change at all.
What could be the issue here?
Your help would be appreciated.