This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020: Possible inductance range

Part Number: TPS63020

My customer will implement following design.

VIN=5V (USB3.0 INPUT) / 900mA
VOUT= 5.2V / 750mA DC MAX (AC MAX 2A for Audio)

My customer is designing with 1uH following Datasheet. Could you please let me know acceptable inductance range(min typ and MAX value)?

Best Regards,
Hironori Yoshimura