Hi,
From the datasheet,
If the SS/TRK pin is floating, the LMZM33606 starts up following the fixed, 5-ms internal soft-start ramp. Use CSS to extend soft-start time when there are a large amount of output capacitors, or the output voltage is high, or the output is heavily loaded during start-up.
The Query is,
Consider the output Capacitor values as min to moderate as 100 uF to 250 uF.
Can I reduce the ramp rate (like 0.1 mS or 1 mS) using the formula (CSS = ISSC × tSS)?