Part Number: LM7480-Q1
Other Parts Discussed in Thread: LM74500-Q1
Hello,
I am using the LM74801QDRRRQ1 in a reverse battery protection / ideal diode application (snapshot below/attached) in an application up to 45V and 70A. Note R117 is not stuffed by default. IPC-2221B clearance requirements are 15.75 mils between component leads/terminations at this voltage (and 23.62 mils between external conductors). After progressing to layout, I have run into some issues with this schematic:
- The datasheet for the LM7480-Q1 says that if VSNS and SW are not used, short them and connect to VS. The OV pin is connected to GND because the secondary HGATE is not used. This places 45V between SW and OV at well less than 15.75 mil. Can any of these VSNS, SW, and OV connections be changed to maintain 15.75 mil clearance between 45V signals? Similarly, if R117 were installed then OV would be too close to the EN/UVLO connection.
- The Figure 9-2 application in the datasheet shows OUT pin 9 grounded. This places OUT next to the 45V connection at VS pin 10. Similar question: can the OUT pin 9 be connected differently?
Alternative questions to the above for my application may be: what would happen if VSNS or SW were grounded? What would happen if OV were connected to VS? What would happen if OUT were connected to VS?