Part Number: TPS40322
Other Parts Discussed in Thread: LM25119
Hello Team,
My customer is working with TPS40322 at voltages bigger than 5.6V (max. permitted in the datasheet). Since this is not applicable they wanted to know if we can suggest a single controller with interleaved outputs because of the lower current ripple and better performances due to lower current (one half) managed by each output. They need to reach about 30A in total and up to 7V output voltage, NOT both at the same time: 30A with 3V laser diodes and 20A with 7V laser diodes.
Regards,
Renan