This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478: LM3478

Part Number: LM3478


Hi, TEAM
Is there any problem with the characteristics of this product even if it is operated at 100KHZ? Do you have data for this product to work at 100KHZ?
Best Regards, BANE
  • Hello Haruo,

    The datasheet gives some typical characteristic graphs for 100kHz, so you can use it at this frequency, it is not very often used at such a low frequency. What is the reason that you want to go such low?

  • Hello Brigitte,

     

    In the datasheet, Fnom is specified min 350kHz, Max 440kHz for typ 400kHz with RFA = 40kohm over temperature.

    In case of typ 100kHz, customer can think Fnom has same variation as well as in case of typ 400kHz ?

     

    Customer worried about entering unstable operation or getting large variation of SW frequency by using 100kHz SW frequency.

     

    Since the RFA has also variation, if SW frequency was configured 98kHz by the resistor variation, LM3478 wouldn’t work...

    The above case might be happened ?

     

    Thank you and best regards,

    Michiaki

  • Hi Michiaki,

    Your analysis here is basically right. As the variation at 100kHz is not given in the datasheet, please leave enough margin when selecting the RFA so that the actual operation frequency is >=100kHz. Otherwise, the performance will not be guaranteed.

    Thanks,

    Yinsong

  • Hello Yinsong,

     

    Customer will have some margin to meet datasheet spec but they are wondering how much variation for SW frequency they should estimate.

    For instance, if they configure SW frequency at 110kHz with margin, how much variation does LM3478 have ?

     

    Customer can use same ratio for the variation, showing 350kHz – 440kHz variation for 400kHz in the datasheet ?

     

    Thank you and best regards,

    Michiaki

  • Hi Michiaki,

    I have asked our designer about this. Let's wait for their feedback.

    Thanks,

    Yinsong

  • Hi Michiaki,

    Sorry but we don't have more information here. The only reference would be the figure 5 curve in the datasheet, which shows a very small variation.

    Thanks,

    Yinsong