This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A47: Change in functionality, stuck at 2.5V and pulls high current

Part Number: TPS7A47

I've use this part on several different designs and never had any issues.

Recently, I did another run of an existing PCB with 2 of these parts, and the outputs are both stuck at 2.5V and pull as much current as I give them (The first set of 12 boards never had any issues.) They should output 3.3V and 5V when provided a 6V or higher input. What has changed, and how do I fix it? I see the issue on both parts on 5 different boards. We tried replacing the parts and still see the issue. Schematic screenshot is attached. The PCBs don't appear to have any shorts, so the issue appears to be related to this LDO.