IS THERE A 12 v version of SN6505 push pull transformer driver?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Robin,
Thank you for posting to E2E!
We do not have a 12V-compatible version of SN6505 at this time, however we do recommend using the configuration shown below with an SN6505 device to isolate power supplies with >5V inputs:
Is this a possible solution for your system? More information about this configuration can be found on the two E2E posts linked here:
Respectfully,
Manuel Chavez
Manuel
that is what we are doing now. However, Ours has several outputs! Driving several floating outputs to drive gate drives, diff amps, Inv opamp( -5V)...etc so a single output xmfr is of no use.
Thnx for confirming our approach.
r