Other Parts Discussed in Thread: LM5145, LM5146-Q1
Hi,
I am considering buying a few LM5145EVM-HD-20A boards to test my application. However, the user guide of this EVM says that the output voltage is regulated at 5V. Can I adjust the output voltage of the EVM to 12V or 24V in any manner?
If this is not possible, could you please suggest similar buck converter EVM boards that have the similar Power rating, Input voltage specification, and adjustable Vout to 12V or 24V?
As a result, my requirement need is as follows:
Vin range: 24V - 72V (range in flexible but Vin,max should be at least 60V)
Power Output: 75W - 150W (any board in this range is good enough)
Vout: 5V, 12V, and 24V (It would be great to have one board with adjustable Vout channel that can be configured to 5V, 12V, or 24V. If this is not possible, 3 different boards will also suffice)
Could you please suggest any TI EVMs that can meet this requirement?
Sincerely,
Kartavya Agarwal.