Dear TI,
We are using this TPS2546RTER IC is one of our RUP (Remote USB Port) design.
I recently received from the field two of these RUP equipped with IC TPS2546RTER burnout. Take note that this is very isolated case (2 out of thousands in service).
I am trying to duplicate this burnout condition by creating a short on the USB port with no success (the IC comes hot (approx 90 degrees C on IC body but do not burn out).
I am trying to identify the root cause but can only suspect a defective IC or liquid contamination (no obvious trace) at this time.
Have you ever seen such a burnout condition and if so, what can be the cause(s) ? Here is a picture so you can see by yourself.
Regards,
Daniel Belzile
Inflight Canada Inc.
Quality Manager