This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1210: Negative Gate-Source-Voltage with the LMG1210

Part Number: LMG1210

Hello, 

my customer has the following question:

At the moment I am working on a 2kW Class-D-Amp with your Driver LMG1210 for GaN-MOSFETs. In my research I read in the application-notes from GaN-Systems, that it is necessary to work with a negative Gate-Source-Voltage  in high power-applications. So my question is: Is it possible to achieve a negative Gate-Source-Voltage with the LMG1210 without losing Voltage in positive switching edge?

 

Thanks 

Jan