Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ10503EXT: Datasheet vs Webench

Part Number: LMZ10503EXT

Hello,

The datasheet for this device has an example for converting 5V to 2.5V (sections 8.2 and 8.3). When I enter the resistor values for Rfbt and Rfbb given in the datasheet into Webench, it complains saying that the values are lower than the minimum allowed. I have two questions regarding that:

1- Which one should I believe more, the datasheet or Webench?

2- It seems that when I change the output current from say 3A to 1A, the two resistors values for Rfbt and Rfbb change quite a bit. Why would that be the case if the output voltage remains the same? Aren't these resistors mostly used for voltage divider purposes?

Thank you in advance for your support

Ray P.