Other Parts Discussed in Thread: UCC28630
We developed a flyback design based on the UCC28631 part. We received the boards and unfortunately, the supply is not starting when applying power. We believe the supply thinks the VSENSE pin is open and enters a pin fault protection mode during power-up. The VSENSE circuit is correct and identical to the EVM design, but the sense resistors' values might be the issue here. We use 40.2k for Ra and 73.2k for RB. The Thevenin equivalent resistance is ~26k, which is above the recommended range (10k-20k) mentioned on page 30 of the datasheet.
Can we change Ra and Rb to fix this issue? Since we are close to the upper limit (26k vs. 20k), we are wondering if we can reduce Ra to 30.9kOhm and Rb to 56.2kOhm. This new combination brings the Thevenin value to 20kOhm and maintains a similar Rb/(Rb+Ra) ratio. However, we don't know if reducing Ra is acceptable. The datasheet lists equation 11 to calculates Ra's value with no explanation of why, so we don't know if we can change it to 30.9k. We think it has to do with sensing Vin. If you can please let us know if this acceptable or if you recommend a different route, that would be great. Ideally, we don't want to change the transformer turn ratio. At least for this rev of the boards. Thx!