This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146-Q1: https://www.ti.com/lit/ds/symlink/lm5146-q1.pdf?ts=1615177629257&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FLM5146-Q1

Part Number: LM5146-Q1

Please refer to the picture attached. For the Regulator LM5146-Q1, the formula for finding the Rlim resistor is mentioned in the datasheet. In the numerator, the minimum current through the low side MOSFET M2 is taken i.e. Iout-delta(iL)/2 .  But since, this circuitry is used for overcurrent protection, we feel that the maximum current i.e.  Iout+delta(iL)/2 should come instead of Iout-delta(iL)/2 in the numerator. I request you to please explain the logic behind  Iout-delta(iL)/2 term in the numerator, because even during the OFF cycle, the maximum current in the below transistor would be  Iout+delta(iL)/2