Other Parts Discussed in Thread: TPS61165
Hi,
I am using the TPS61165EVM to drive an LED bar that is external to the module. The TPS61165EVM is designed for an input voltage of 5V ± 10%. I would like to use a different range, from 3V to 7V. Which components should I change?
BR,
Gloria