This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165EVM-283: How to expand the input voltage range of the TPS61165EVM

Part Number: TPS61165EVM-283
Other Parts Discussed in Thread: TPS61165

Hi,

I am using the TPS61165EVM to drive an LED bar that is external to the module. The TPS61165EVM is designed for an input voltage of 5V ± 10%. I would like to use a different range, from 3V to 7V. Which components should I change?


BR,

Gloria