This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400-Q1: What is the operating Junction temperature of TPS65400-Q1

Part Number: TPS65400-Q1
Other Parts Discussed in Thread: TPS54331, TPS54231, TPS54335A, TPS560430-Q1

Hi, 

AEC Grade 1 means the ambient temperature is -40 to 125°C.

So the operating junction temperature should be above 125°C due to the power dissipation in the IC.

But in TPS65400-Q1 datasheet the operating junction temperature is mentioned as -40 to 125°C which is conflicting the AEC Grade 1 standard.

Please clarify the what is the correct operating junction temperature range.

This is very critical for our design to qualify this IC.