Other Parts Discussed in Thread: BQ34Z100, GPCCHEM, BQ34110, BQSTUDIO
hello,
We just completed the relax discharge relax process to determine the chemical ID. regarding the reports received, we have some questions:
"Best chemical ID : 436 Best chemical ID max. deviation, % : 13.78" //Chemical ID deviation is 13%.What is the Impact on SOC accuracy and SOH accuracy using Lifepo4?
"Summary of all IDs with max. DOD deviation below 15%
Chem ID max DOD error, % Max R deviation, ratio
436 13.78 1.22
421 14.31 0.76" //What would be the creterias that would make us choose another chem ID?
"Selection of best generic ID for ROM based devices like bq274xx
Device / Family #1
Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % //why is it only speaking of LiCoO2 technology and bq27? We'd like to use a bq34z100-g1 on Lifepo4 technology.
128 bq27421-G1A: 4.2V LiCoO2 1707.38
3142 bq27421-G1D: 4.4V LiCoO2 1844.43
354 bq27411-G1C: 4.35V LiCoO2 1872.32
312 bq27421-G1B: 4.3V LiCoO2 2157.65
Best generic ID 128
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule"
And more:
- Our application go further than 30Amps, therefore, we have a lower shunt resistor (250µOhms). I guess the accuracy of the calculations will be diminished, can we know how much?
- if we understood well the SLUA450 Document, OCV is the main parameter to define the Ra table and Qmax. After a long shutting of period of our system, When it wakes up, does the bq34z100 give an approximate value of the SOC with only an OCV measurment?
Thank you verry much for your help