Other Parts Discussed in Thread: SN6501
Hey,
I am trying to use UCC27284 as a high-side battery switch to replace the relay. I have the following questions:-
1. When making a 48V battery switch for 100A, should I provide isolated power to UCC27284, or can a nonisolated supply also work for the same.
2. for driving the gate above its vth and to operate in saturation region I wanted to understand how will that be done ( do i need a charge pump circuit or can it operate without the same), as I am using this article as a reference so far. (https://www.ti.com/lit/an/snvt010a/snvt010a.pdf?ts=1615367452699&ref_url=https%253A%252F%252Fwww.google.com%252F)
3. Also should I have an active freewheel circuit or a passive one is good enough, a bit worried about the heating of the system.
Thanks in advance.
Naman