Other Parts Discussed in Thread: CSD87353Q5D
Hello!, I have some Question about LM5175 and Dual Power Mosfet.
I develop the Buck-Boost Power Module using the LM5175 IC. this is very work well.
<Buck-Boost Power Module Spec of My Mainboard>
1. Input : 9V~36V
2. Output Voltage : 12V
3. Output Current : 5A
4. Mode : DCM + Hiccup Enable.
5. SW freq : 330KHz
** I have to design the Mainboard and i will on-board design the LM5175 Power System.
And the main board size I designed is a small form-factor. That's why small form-factor size components should be used to reduce the main board size.
<Question>
1. It is okay about i using the dual Power Mosfet in LM5175 Power schematic?
2. Are there any dual Mosfet (Ti Vendor) products to recommend?
** Currently, My LM5175 schematic designed single Power Mosfet *4 EA, in the my Mainboard.
so i would like exchanged single power Mosfet to Dual Power Mosfet(Ti Vendor)
If you give me a reply, i really appreciate.
Thank you!