This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2677: Equivalent Circuit to LM2576 1.2-30V 3A Circuit

Part Number: LM2677
Other Parts Discussed in Thread: LM2576,

In the LM2576 datasheet there is a circuit (Figure 23) which has an fixed input voltage and supports an adjustable output voltage over a wide range without changing component values.  Since I would presume that if you supplied something like fixed 36V to the input and possibly adjusted the feedback resistors value somewhat, you could change the 1.2-50V range to a 1.2-30V that doesn't require the more expensive HV version.  Would the LM2677 support a similar circuit with  36Vin & 3-30V adjustable range but 5A out rather than 3A, i.e. Is there a set of LC components that matches the required ExV value(s)?  

Thank you!