If an LM2596 is used to charge, say, a 12V lead acid battery, and the input comes from, say, a 36V solar panel that will generate no voltage during the night, is it necessary to protect the LM2596 against the battery voltage when no input voltage is present?
The data sheet does not include a spec for Vbe max of the internal NPN switching transistors. If this was >14V I think no such protection would be needed. If it is less than 14V then a Schottky diode between output and battery would be needed.
(Yes I know there are bespoke MPPT chips, but I have my reasons for contemplating LM2596 use here)