Other Parts Discussed in Thread: TPS23758EVM-080
Hi,
My customer wants to build a power delivery solution for a PD. The final the design has to be very flat:
- Height final design <10mm
- Input Voltage Range - conform to 802.3 af/ at max 13W
- What type of input source it is - 802.3 af/ at conform power source
- 0utput voltage - 5V or 12V or multirail for 1.8V, 3.3V, 5V/ 12V
- What the output rail will be powering - analog amplifier, DDR2, microprozessor
- Isolation needed - yes according to 802.3 af/ at
- Efficiency >80%
- Output Ripple <50mV
- switching frequency >250kHz
What devices/ reference designs do you would recommend for that.
Thanks
Jan