Other Parts Discussed in Thread: BQ25505
Power input: 1V, 20mA average
Power storage: 500mAh Li-poly battery, rechargeble
Desired Power output: 3.3V, peak 500mA (may last 5ms), average 1mA.
Can bq25570 supply 500mA peak for short time?
From spec page 17: "The converter delivers an output current up to 110mA typical".
yet page 24 has show an example to output 500mA with enlarged Cstor.
Could you help clarify whether and how can I achieve the desired output?
And if not feasible with BQ25570, will any other chip like bq25505 can fulfill?