Part Number: LM2991
Hi,
I am using LM2991 with Vin = -5V, Vout = -2V, Iout = 0.3Amax now.
However, to fix the problem, I need to use the LM2991 Vout at -1.55V.
When I refer to the data sheet, Vout is typ -2V, but there is no value for min.
Since Vref = -1.21V, I think it is possible to output Vout = -1.55V, is that correct?
I think of R2=750ohm and R1 = 2.7kohm. And my circuit current is 40mA min, so minimum load is no problem.
Regards,
Ikuo