Part Number: TPS563210A
Hi team,
Please let me ask questions about EN-pin from customer.
1. Looking at Recommended Operating Conditions, it is OK to apply 17V to EN-pin. Is this true?
For example, is it OK to apply 15V to EN-pin when Vin = 12V?
2. They consider to add RC filter in front of RC filter. Are there any limitations regarding rising/falling edge for EN-pin?
3. EN pin resistance to GND is 225kOhm(min) to 900kOhm(max) when V_EN = 12V. Can this resistance be varied when V_EN is also different?
If the resistance will be varied, could you provide any data or trend of the value?
Regards,
Noriyuki Takahashi