This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM350A: Need to generate 125mA load current

Part Number: LM350A
Other Parts Discussed in Thread: TPS7A26, TPS7A25, TPS7A24

Hello Guys,

Good day.

Our customer is using LM350A on their design. They have a 12V source and load with resistance of 80ohms. They need to generate current with this load at 125mA. How can they achieve this?

When they increase Vin to 15-16V, device can generate 125mA but not at 12V source. Any alternative part is welcome too.

Thanks in advance!

Art