Part Number: LM4041C
Other Parts Discussed in Thread: TL431
LM4041 ADJ regulator in TO92 package. Wired with anode to return, 10K ohms from adj to return, 47K ohms from cathode to adj, 2K ohms from cathode to positive supply (7 - 8.5 volts), careful not to exceed 10 volts. Should regulate to about 7 volts; measured approx. 1.5 volts at cathode, about 0.4 volts at adj. Problem observed with multiple parts. Even if positive supply is insufficient, should not see such low voltages!
Pinout used: TO-92 facing the flat surface, leads down: adj on the left, cathode in the middle, anode on the right.
Parts are marked:
(N)07111
4041C
IZADJ
where (N) is the old National Semiconductor logo.
Parts were purchased 2 Mar 2021.
I really think these parts are defective; I got my circuit working with TL431.