Hello,
We have an application where the system pulls ~6A, we have a battery in the system to allow for a safe/slow power down once the input supply is gone.
We need a simple battery charger ~500mA to charge the battery, it will sit at full charge most of the time. But when the input supply falls the battery needs to supplement the system while it shuts down.
The BQ25050 has an external FET which is useful as 6A won't work on an integrated FET. But most of our chargers have the input --> output through the device which also presents a current limitation.
Can the BQ25050 be used in the below way to bypass the OUT pin (bypass the internal IN-->OUT FETS) while still providing it the necessary information to switch over to the battery when the input supply falls? The resistor is there to current limit the OUT pin but still provide the voltage sense functionality.
Thanks,
Nick