This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568: The soft start time min value / max value

Part Number: TLV62568
Hello experts,
The TLV62568DRL data sheet states that the soft start time at Tj = 25 ° C is 0.9ms (typ).
Please tell me the soft start time min value / max value when Tj = -40 to 125 ° C.
Soft start time (Tj = 25 ℃)
Typ value = 900us
<Confirmation details>
Soft start time (Tj = 125 ℃)
Min value = confirmation time
Max value = confirmation time

Thanks and best regards,

-Udai

  • Hello Udai,

    Thank you for your question.

    I am sorry, but we don't share this kind of data on this platform.

    If needed, please contact your local TI sales team in order to discuss this topic privately.

    Just an additional comment; it's very difficult to tell you meaningful limits for the soft start time because, since it includes also the rise time of the output voltage, it strictly depends on your circuit parameters, as COUT, VOUT, inductor value, VIN, …

    Thank you,

    Stefano

    All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml).

  • Hello Stefano,

    Thanks for the reply.

    I will talk to the TI sales team about this question.

    Thank you,

    Udai