Other Parts Discussed in Thread: BQWIZARD, BQSTUDIO
Hi,
Please help me in finding the updated Firm Ware of the BQ78PL116. As I am seeing different Firmware files in BQ studio tool.
Thanks & Regards,
Uday Kumar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi shirish,
It is just a name mention mistake because I was working on both impedance gauge IC and BQ78PL116. I am using BQwizard 3.1 version.
I am seeing FW versions of 6000 and build version 719 and 720 and 810 and 727(in BQ78PL116R1). In different versions of BQwizard tool (3.1)and 3.4).
Load the latest version of bqWizard from the web.
The instructions to follow to load the F/W is as follows:
To load new firmware
- Go to Bootstrap Loader dialog box: Main menu --> Utilities --> Bootstrap Loader
- Click on "Select File" button
- Browse to "C:\Program Files\Texas Instruments\bqWizard 3\Configuration Files\bq78PL116\Firmware"
- Select FW_0002_0000_6000_0719.enc "Open"
- After returning to Bootstrap Loader dialog box select "Preserve Calibration" box
- Click on "Download" button
- Save calibration data to a file
- After download is complete, approximately 50s, close the Bootstrap Loader dialog box. Control returns to the bqWizard
- Read all parameters: Main menu --> Commands --> Read All Parameters
- Turn on "Wired bit": Main Menu --> Commands --> Toggle Wired Bit
This should update the bq78PLPL116 to the latest F/W revision.