Hello,
I'd like to confirm my understanding of the RS-CONF resistor limits. I have an application which requires an 18.2 kOhm configuration setting. Unfortunately, I only have 18.0kOhm in my design library.
Given the EC table:
-
Would it be safe to assume that the acceptable limits are 18.2kOhm +/- 4% = 17432 Ohms -> 18928 Ohms
Thus if I use an 18.0kOhm 1% resistor (17820 Ohms -> 18180 Ohms), it will fall safely within those limits?
Don