Other Parts Discussed in Thread: TPS61094
Hello,
I'm starting a new board and a high efficiency voltage regulator is needed with the following main specs:
- Vin [2V - 3.7V]
- Vout [3.3V]
- Iout [10uA - 400mA]
I was tending to use TPS63900 since it has stock available in Mouser. However, I saw it is out of stock in TI website.
TPS61094, on the other hand, has 4000+ units available in TI website, but is not available in big stores (probably because it's a new device, right?).
Questions:
Will TI keep producing TPS63900? Which one would you recommend for new designs, given that we'll need 1000+ pieces in the next 1 - 2 years?
Suggestions of other devices that can meet our specs are welcome.
Thanks for helping,
Bruno