Other Parts Discussed in Thread: TPS25947, TPS2596,
Hi,
Before TPS259570 enable, customer use E-load to apply 1.6A at CC mode. Then enable the TPS259570 and found there is no output. But when the E-load set to CR mode, the output is normal.
If we reduce load to from 1.6A to 1A at CC mode, the output is normal.
Is that trigger inrush current protection or something?
System setting:
Vin = 3.3V
Vout =3.3V
Iout = 1.6A
ILIMIT ~= 4.17A (RILM = 487 Ω)
E-Load is set to CC mode:
CH1:Vout, CH2: Vin, CH3: EN, CH4: Iout.
E-Load is set to CR mode:
CH1:Vout, CH2: Vin, CH3: EN, CH4: Iout.