Hi team,
Here come across some LM1117 chips output voltage ripple too much case need your help to guide whether what is risk/potenial reason with below schematic or layout ? if moved the not working fine chip to other w/o LED board, the output is normal without such high ripple.
C87-C88: 100nF±10%-50V-0603-X7R
C164: 10nF±10%-50V-0603-X7R
C156:10uF±10%-16V-1206-X7R
R197:1/10W-1KΩ±1%
LED1 :80 mW