Hello Guys,
Good day.
Our customer have a few questions on TPS7H4010-SEP, which we are hoping you could help.
1) Can this device provide a -3.3V output with a Vin of +12V? In other words can it provide a negative voltage with respect to the input voltage?
2) Also please check if it can output -3.3V when the input voltage is +28V.
The idea is to connect the Vout pin to system ground (0V) and then the return pin becomes the negative output voltage.
Thanks in advance!
Art