Hi Team,
My customer is design PROGRAMMER system for TPS65217, would team help to check the schematic?
Can customer flash and read TPS65217 only provided input voltage?
Thanks & Regards
Eddie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer is design PROGRAMMER system for TPS65217, would team help to check the schematic?
Can customer flash and read TPS65217 only provided input voltage?
Thanks & Regards
Eddie
Hi Eddie,
Can you provide more details on your use-case? From the schematic you uploaded, it is not recommended to leave all of those outputs NC. You can find a suggested schematic review checklist here as well.
Best,
Emily
Hi Emily,
The application is PROGRAMMER tooling for TPS65217, customer provide PROGRAMMER services for our TPS65217 customers.
Do they still need connect output pins?
Eddie
Hi Eddie,
The TPS65217 can be powered up with nothing connected to the outputs only if all the regulators are disabled.
Best,
Emily
For further clarification, the TPS65217 will turn off after 5s if the PWN_EN pin is not set high. During WAIT_PWR_EN state, LDO1 will be ON and all other rails will be off. While it is possible to re-program the device within this 5s window, it would have to be an automated process.