The CPU solution is denverton, and the vid version is vr13,
The requirements are as follows: the maximum power consumption is 30W, and four power supply channels are required.
Pvcc 1.05v 30A svid_ addr=0x00
Pvnn 1.05v 10A svid_ addr=0x01
Pvddq 1.2v 10A svid_ addr=0x02
Pvccsram 1.05v 10A svid_ addr=0x03
After discussion with customers, we recommend tps53622rsbr 2-way, and the MOS selects 1pcs csd95495qvm + 3pcs csd95492qvm or 5pcs csd95492qvm.
. please help to see if the recommended solution tps53622rsbr csd95495qvm csd95492qvm has a better choice