When I searched TPS7A52 in the PSpice for TI tool, I only see one simulation model is available, and that is for TPS7A52-Q1 with 3 in pins and 3 out pins. However, the one I want to use is the TPS7A52 model. Will this model be updated by TI? Or do I need to import it from other sources? P.S. The version of PSpice for TI tool I am using is 17.4-2020 S004 Windows SPB 64-bit Edition.
Thanks.