The Excel TI Thermistor Coefficent Calculator does not work for BQ34110 as the BQ34110 data sheet and technical reference manual do not specify R1 or R2.
As an example the datasheet says that the default data was calculated using a Semitec 103AT thermistor.
This data from the default config for the chip itself is:
coeff 1 20982
coeff 2 -13836
coeff 3 5202
coeff 4 233.7
However using the Semitec example data from the spreadsheet does not generate anything close to those numbers.
It doesn't appear possible to re-create the default data in the BQ34110 using the Thermistor Coefficient Calculator Excel file.
Any ideas?
I am using NTCLE400E3103H thermistor.