My proposed application, in a battery-operated design, uses a pull-up resistor for the enable pins on the LM27762, that is grounded when powered off. It is important to the application to minimize the current draw when the device is off.
Unfortunately, I was unable to find any specs on the enable pin current requirements, or on its effective input resistance. Without WEBENCH, I'm unable to simulate this.
Can you tell me, please, how much current is required to enable the output? Alternatively, would you have a suggested value for a pull-up resistor that would supply adequate current to keep that pin above the 1.5V threshold when connected to a 3.5V source?
Thanks for your help.
I'd also be grateful to anyone who would care to comment on this layout. 0805 resistors were used for programming (R2 and R4 in my schematic), simply to make it easier to alter output voltage by hand.