Other Parts Discussed in Thread: TPS61288
Hi expert,
I am trying to adjust to apply the TPS61228 for a single cell battery input to work between 2.7V to 4.2V, and Vout around 12V.
I have got a TPS61288EVM-064, the default output is approx 12V when unloaded, but the output starts to become unstable when loading more than 1A
and used WeBench to generate a design.
The designed schematics gave a different value for Rc, Cc and Cp, and I have tried them on the EVM,
However the output of the EVM cannot support more than 1A with a 3.0V input.
an you give me some guidance where i might have missed out something important?
thanks!
-