POINT 1
Customer wants to change the voltage setting in the internal NVM.
The DS states:
It is permitted to use the STORE_DEFAULT_ALL command while the device is operating.
However, the device may be unresponsive during the write operation with unpredictable memory storage results.
TI recommends to turn the device output off before issuing this command.
It will be difficult for my customer to turn the output off while device is operating to use STORE_DEFAULT_ALL, as they would end up violating their power startup sequencing.
1) What is the fail rate for writing change to NVM with Output OFF vs ON?
2) If the NVM write fails, is there any impact to info stored on RAM? (= device operational conditions)
3) After a fail, can NVM be written again?
4) Is there any way to write NVM without applying voltage to PVIN pin? (ex: Can PMBus features operate with voltage only on BP or VDD?)
POINT 2
It seems we need to set R_VSEL=OPEN/0Ω/1.78K/187K in order to set VOUT_COMMAND with NVM.
I understand this sets InitialBootVoltage to 0.975V.
Is there any chance the InitialBootVoltage is actually used for an operation condition?
If so, is 0.975V the only InitialBootVoltage that can be set?
If so, at what timing does the change from InitialBootVoltage to the NVM setting happen?
Regards,
Darren